MOVE UP TO DIGITAL SPRING REBATE Motorola Solutions recognizes the challenges you face with rapidly escalating costs that results in tighter budgets. Motorola two-way radios are the answer, allowing your team to accomplish the same, with less. All Motorola business models are designed to enable clearer communication and easier usage, to the virtually uninterrupted performance on the job. Plus, Motorola offers ergonomic design, crisp audio quality, long-lasting battery life and are all narrowband compliant. CLP SERIES RADIOS The CLP’s small, unobtrusive design packs a big punch in a lightweight, palm-sized package and offers some of the most reliable communications in even the noisiest of environments. The CLP1060 six-channel radios are Bluetooth™ capable. The CLP single- and four-channel models feature wired headphones. All CLP Radios bring a choice of 90 UHF business-exclusive frequencies. They are easily operable and come standard with push-to-talk functionality and an extended battery life. These radios meet military standards for shock, vibration, temperature and antimicrobial protection. CLS SERIES RADIOS Rely on impressive coverage capability in this compact radio. It operates on 56 businessexclusive frequencies and includes a coverage range of up to 200,000*** square feet with the choice of either single- or four-channel models. Intuitive and user friendly, the CLS streamlined design is fronted by a crystal-clear LCD display. The CLS (Clear, Light, Simple) Series meets military standards for shock, vibration, temperature and antimicrobial protection. DLR SERIES RADIOS The lightweight, sleek Motorola DLR digital radio provides a simple but powerful collaboration tool and allows the flexibility to configure the radios to meet your procedural needs and optimize staff experience. The license-free DLR features multiple call options which can enhance communications between team members, as well as frequency hopping technology designed for increased security. Talk Permit Tone lets users know when the channel is free for them to talk, therefore promoting orderly communications. Voice prompts allow easy navigation of menus, channels, battery status and more. The Home Channel feature automatically returns users to their primary channel when a conversation is over. DTR SERIES RADIOS The DTR Series digital radio works wherever people do. Reporting from the production line or the principal’s office, you’ll enjoy expanded in-building coverage – up to 350,000*** sq. ft with the standard whip antenna. Digital audio quality stays loud and clear – up to the edge of coverage – without static or dead zones. Compact, durable, and IP54 rated design meets U.S. Military 810G standards for shock, vibration, water, dust and temperature extremes - so it will operate in the harshest working conditions. Other key features include interference free and private communications, vibrant color display, flexible call options, and license free operation. RD SERIES RADIOS Introduce your workers to the perfect business partner that will help make any workplace environment more productive for them and more financially rewarding for you. Not even some of the harshest job-site conditions stop the affordable, easy to use RD on-site business radio. Enhanced wattage extends coverage to up to 350,000*** square feet (4/5 watt radio models). Its outstanding industrial design features a heavy-duty metal body that meets military standards for shock, vibration, water, dust and temperature, and protects its premium performance: exceptional audio quality, easy programming of frequencies and radio settings, advanced voice activation, flexible battery life solutions, and easy cloning. RM SERIES RADIOS Empowering your workforce with a reliable, long-lasting audio solution is the hallmark of the RM Series. Capable of customizing channels per radio via voice alias, the RM has a coverage range of up to 250,000*** square feet and can operate on either four or eight channels, across each UHF, VHF and MURS frequency. Count on up to 12-hour battery life without the Battery Save feature and up to 15-hour battery life with the Battery Save feature. The RM Series radios meet military standards for shock, vibration, water, dust, temperature and antimicrobial protection and provides NOAA weather alerts. PROMOTION TERMS & CONDITIONS: 1. Promotion valid only on the following qualifying Motorola Solutions (“Motorola”) new condition Two-Way Business Radios (“Eligible Radios”) purchased by a legal business entity from a Motorola Authorized Business Radio Reseller between March 1, 2020 – June 30, 2020. (“Promotion Period”). ANALOG RADIOS: CLP Series (CLP1010, CLP1040, CLP1060), CLS Series (CLS1110, CLS1410), RD Series (RDU4100, RDV5100, RDU4160d), RM Series (RMU2040, RMU2080, RMU2080d, RMM2050, RMV2080). DIGITAL RADIOS: DLR Series (DLR1020, DLR1060) and DTR Series (DTR600). Promotion excludes DTR410, DTR550, DTR700 (a commercial radio), any models discontinued by Motorola, and all bulk (non-packaged) purchase models, pre-owned/used condition purchase models, and rental fleet purchase models. 2. The end-using business entity that made the purchase (“End-User”) will receive one free radio with each qualified claim of six (6) analog same-series radios; and one free radio with each qualified claim of five (5) digital same-series radios (up to the maximum qualifying limit). 3. End-User can purchase as many eligible radios as needed, but the promotion will be limited to a maximum of sixty (60) total qualifying purchased radios claimed per customer/company. Additionally, no single customer location can redeem more than the maximum qualifying limit. 4. To receive the free rewards (up to the maximum qualifying limit), End-User must completely fill out the online claim submission form available at www.MotorolaSolutionsRadioRewards.com,and supply all requested documentation. All claims will be validated, and online claim information and supporting documentation must match. 5. Claims, including valid and complete supporting documentation, must be entered by 11:59 pm EST on Monday, July 20, 2020 (“Expiration Date”). No exceptions will be made for expired claims. 6. Total qualifying purchases (up to the maximum limits) may be claimed in one or more submissions, and must be grouped in any combination of six (6) CLP, six (6) CLS, five (5) DLR, five (5) DTR, six (6) RD, or six (6) RM Series two-way radios. 7. Proof of purchase (sales receipt or invoice) is required, and must be dated during the promotion period. Multiple sales receipts/invoices allowed per claim. The Authorized Reseller that issued the invoice/sales receipt must be the same Authorized Reseller entered on the online claim submission form. Pick tickets/packing slips are not acceptable. 8. FREE RADIO: End-User will be rewarded the qualifying radio model with the lesser value of each qualifying group of six (6) CLP, CLS, RD, and RM same-series radios claimed, and each qualifying group of five (5) DLR and DTR same-series radios claimed. In the event that there are multiple qualifying radio models claimed with the same lesser value, Motorola will be solely responsible for determining the lesser value radio model(s) rewarded per group of qualifying same-series radios. Promotional value for each qualifying radio reward is: CLP Series Radios (CLP1010 is $219, CLP1040 is $249, CLP1060 is $369), CLS Series Radios (CLS1110 is $189, CLS1410 is $209), DLR Series Radios (DLR1020 is $239, DLR1060 is $259), DTR Series Radios (DTR600 is $369), RD Series Radios (RDU4100 is $360, RDV5100 is $325, RDU4160d is $380), RM Series Radios (RMU2040 is $245, RMU2080 is $290, RMU2080d is $310, RMM2050 is $225, RMV2080 is $245). 9. Please allow 6-8 weeks from receipt of a valid and complete submission to receive your free product(s). Products rewarded from the same submission will ship at the same time. 10. Rewards cannot be mailed to a PO Box or residential address. A residential address is considered a home, apartment, or other dwelling where people live on the premises. Claims and profiles with a PO Box or residential address may be rejected. 11. Reward returns/exchanges: End-User must process a return with the rebate support center for any non-working, damaged or incorrectly fulfilled rewards within thirty (30) days of the delivery date to receive a replacement reward. For undeliverable rewards, End-User must notify the rebate support center that the reward was not received within 60 days of the ship date to receive a replacement. Exchanges are not allowed after a reward has been fulfilled or shipped. 12. For promotion questions, call the rebate support center at 1-844-539-5509 from 9am-5:15pm EST or email MotorolaSolutionsRadioRewards@acbcoop.com. 13. No cash will be provided. No extended delivery dates are allowed under these offers. 14. Promotion is valid only in the U.S. and Puerto Rico and is void where prohibited, taxed or restricted by law. 15. This promotion may not be combined with any other promotional offers, rebates, coupons or discounts. This promotion is not transferable. Any requests that do not comply with the terms of this promotion will be rejected. This promotion is subject to all local laws and regulations. 16. Motorola is not responsible for lost, late, mutilated, misdirected or postage due mail (paper or electronic), and shall not be responsible for any shipping or invoice delays. Eligible radios purchased and subsequently returned for refund are not eligible for the promotion. Duplicate requests will not be considered. 17. Motorola and its agents have the right to audit, validate or verify any purchases claimed, serial numbers submitted, and any other information associated with the End-User’s promotional profile and claims. Motorola and its agents also have the right to require additional validating information that may not have been required at the time of claim or profile set-up. If any information cannot be validated by Motorola or its agents, the End-User’s claims will be rejected and the profile may be deactivated. 18. The submission of false, incorrect, misleading or fraudulent information or documentation could result in disqualification from this and future Motorola promotions, and criminal activity will be referred to the appropriate authority for action. 19. Motorola reserves the right to modify, withdraw or cancel this promotion at any time, with or without any prior notice. Please make a copy of all materials submitted. 20. This offer is subject to product availability. 21. The reseller cannot claim the rebate(s) on behalf of the End-User. 22. The individual submitting a claim acknowledges that, by submitting a claim, he/she is authorized to receive any qualifying rewards on behalf of and for use by the End-User; and that any qualifying rewards are not intended as a gift, contribution, or benefit to the individual, any government officials or employees, or any other individuals. 23. Motorola is not responsible for misuse of any rewards by officials or employees of the End-User and, to the extent permitted by law, the End-User agrees to release and hold Motorola harmless with regard to the End-User’s participation in the promotion, and acceptance and/or use of any rewards. ***The communication range quoted is calculated under optimum conditions, with an unobstructed line of sight. Actual range will vary depending on terrain and other local conditions, and is often less than the maximum possible. Your actual range will be limited by several factors including, but not limited to, terrain, building construction, weather conditions, electromagnetic interference, and obstructions. Motorola Solutions, Inc. 500 West Monroe Street, Chicago, IL 60661 U.S.A. motorolasolutions.com MOTOROLA, MOTO, MOTOROLA SOLUTIONS and the Stylized M Logo are trademarks or registered trademarks of Motorola Trademark Holdings, LLC and are used under license. All other trademarks are the property of their respective owners. © 2019 Motorola Solutions, Inc. All rights reserved. 11-2019
Download PDF file