Reduce the Risk of Concussions Dropped Objects The goal in dropped object prevention is simple. It’s all about trapping, tethering, and topping. Regardless of the method, the goal is always to use anchor points to retain tools and equipment to prevent drops. ANSI/ISEA 121-2018 is a standard that consists of design, testing, performance, and labeling requirements for tool tethering systems and containers used to transport and secure tools and equipment at heights. The four categories of equipment covered in the standard are: • Anchor attachments • Tool attachments • Tool tethers • Containers The requirements of this standard will create formal distinction of a proper tethering system compared to duct tape, string and other inferior solutions. ANSI/ISEA 121 is to dropped object prevention equipment what ANSI Z359 is to fall protection equipment. What is a Concussion? A concussion is a type of TBI caused by a bump, blow, or jolt to the head or a hit to the body that causes the head and brain to suddenly move back and forth. Movements like these can cause the brain to bounce or twist in the skull creating chemical changes that can damage brain cells. Did You Know? National Concussion Awareness Day is held annually in September. http://nationalconcussionawarenessday.com/index.html What to Look For Signs and symptoms generally show up soon after the injury. However, you may not know how serious the injury is at first and some symptoms may not show up for hours or days. Concussion Danger Signs • One pupil larger than the other • Drowsy or unable to wake up • Constant headache that increases • Slurred speech, weakness, or numbness • Vomiting or nausea, convulsions or seizures • Unusual behavior like confusion, agitation, or restlessness • Loss of consciousness, even briefly, should be taken seriously Concussion Signs Observed • Can’t recall events prior to or after a hit or fall • Appears dazed or stunned •Forgets an instruction, is confused about an assignment or position or is unsure • Moves clumsily, talks slowly • Shows mood, behavior, or personality changes Concussion Symptoms Reported • Headache or “pressure” in head • Nausea or vomiting • Balance problems, dizziness, double/blurry vision • Bothered by light or noise • Feeling sluggish, hazy, foggy, or groggy • Confusion, concentration, or memory problems SOURCE: cdc.gov/headsup/basics/concussion_symptoms.html Talk Date:______________________________ Supervisor/Facilitator:_______________________________________ Location:_______________________________ Department:______________________________________________ SAFETY FOR TECHNICAL SUPPORT CONTACT: SAFETYQUESTIONS@FASTENAL.COM OR 1-833-FNL-SAFE WF_357550 JP 09/21 20.7
Download PDF file